Newsletter
02/2024
 
 
Dear reader,
 
Spring is just around the corner and with it the exciting time of trade shows and exhibitions! Today we are pleased to present our latest innovation: the new indexing plunger with chamfered pin. In addition, we would like to inform you about an extension to our range of magnets.
 
Find out which trade shows we will be attending in March and get to know our new products up close.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Indexing Plungers GN 824 with Chamfered Pin
 
Indexing plungers GN 824 have a plunger pin with square cross-section, a latching surface on one side and a chamfer on the other. When the object to be secured moves towards the chamfer, the plunger pin is pushed back into the guide, allowing grooves and edges to pass over the pin. The latching can be released by pulling the knob.
 
Type C / CK indexing plungers with rest position are used for applications when the plunger pin is temporarily not to engage. In that case, the knob is retracted and afterwards turned by 90°. A notch keeps the plunger in this position.
 
More Information!
GN 824
 
 
 
NEW  Retaining Magnets and Holding Disks in Hygienic Design
 
GN 5080 Combi
Retaining magnets GN 5080 and GN 5090 are designed for use in hygienic areas. The sealed screw-on surface enables mounting without dead spaces; the impervious geometry in combination with the high quality finish prevents dirt from accumulating and facilitates cleaning.
 
Holding disks GN 7080 and GN 7090 are used as counterparts for retaining magnets when these are used in combination with non-magnetic materials or when the holding force needs to be increased due to thin material.
 
Take a look!
 
 
 
Upcoming Trade Shows
 
We look forward to seeing you at the following trade shows, where we can offer personalized advice and demonstrations of our products.
We will be exhibiting at the following trade shows in March:
 
all about automation in Friedrichshafen
03/05/25 - 03/06/24
Hall B2, Booth 317
 
Anuga FoodTec in Cologne
03/19/24 - 03/22/24
Hall 8, Booth E 034 / F 037
 
Prolight & Sound in Frankfurt
03/19/24 - 03/22/24
Hall 12.0, Booth E90
Trade Shows
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter