Newsletter
04/2024
 
 
Dear reader,
 
In today's Newsletter we are happy to present our latest product: the spiral cam lever GN 9027 made of high-quality steel. We would also like to draw your attention to the fact that our popular ball joints GN 782 are now available in a stainless steel version.
 
Take the upcoming trade shows as a unique opportunity to discover not only our above-mentioned products, but also a wide range of exciting new products.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Spiral Cam Lever GN 9027
 
Spiral cam levers GN 9027 are used to quickly clamp fixture and machine components with high clamping forces, independent of the direction of the lever. The pitch of the double-sided clamping spiral creates a self-locking effect.
 
Due to the robust design, the lever can be extended by attaching a tube or brought into the desired clamping position by using a soft-face hammer.
 
More Information!
GN 9027
 
 
 
NEW  Ball Joints GN 782 in Stainless Steel
 
GN 782
The clamping nut of the ball joints GN 782 can be set to give a required thrust on the Belleville spring washers in order to increase the resistance to the ball movement.
At the same time the Belleville spring washers act as safety washers for the screws.
 
Ganter is now expanding its range of ball joints with models made of high-quality stainless steel.
 
Learn more!
 
 
 
Upcoming Trade Shows
 
We look forward to seeing you at the following trade shows, where we can offer personalized advice and demonstrations of our products.
We will be exhibiting at the following trade shows:
 
IFAT in Munich
05/13/24 - 05/17/24
Hall C1, Booth 304
 
ACHEMA in Frankfurt
06/10/24 - 06/14/24
Hall 11.0, Booth C 35
Trade Shows
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter