Newsletter
05/2021
 
Standard Parts. Ganter.
 
Dear reader,
 
The smallest of areas on equipment can contaminate entire production lines. For this reason, Ganter has expanded its Hygienic Design product family by adding one additional standard part.
All standard parts of this product family combine high surface quality, free from dead space and bacteria accumulation on outer surfaces as well as sealed mating surfaces.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  GN 1582 Stainless Steel Screws in Hygienic Design
 
Captive stainless steel screws GN 1582 with recessed stud for loss protection expand the product family Hygienic Design. The sealed mounting surface enables components to be mounted without dead spaces.
 
Due to the recessed stud, they are easily secured against loss, such as in a cover.
 
More information about Hygienic Design can be found in the current Highlights brochure.
GN 1582 Stainless Steel Screws, Hygienic Design, Low-Profile Head, with Recessed Stud for Loss Protection
 
 
 
NEW  GN 738.5 Stainless Steel Magnetic Plugs
 
 GN 738.5 Stainless Steel Magnetic Plugs
Stainless steel magnetic plugs GN 738. 5 attract iron particles which might be floating in the fluid. The stainless steel makes them suitable for use in particularly aggressive environments.
 
The outer diameter of stainless steel threaded plugs is matched to screw-in holes for pipe fittings according to DIN 3852.
 
Learn more. . . 
 
 
 
Application Video  GN 251.2 Setting Bolts
 
Setting bolts GN 251. 2 with limit switch are supplied with a hardened rounded head which serves as a firm end stop.
 
When the workpiece contacts the bolt head, an electrical signal is transmitted by the limit switch.
 
Watch our new application video to see how these setting bolts can be used.
Application Video GN 251.2 Setting Bolts
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter