Newsletter
02/2025
 
 
Dear reader,
 
In the second newsletter of this year, we present our new sensor holders GN 801.3 and GN 801.4 - now available as practical accessories for our toggle clamps. In addition we have expanded our range to include the rail mounting clamps GN 474.2, which offer secure fixing and easy handling.
 
Find out at which trade shows you can meet us soon to checkout our products up close!
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Sensor Holders GN 801.3 and GN 801.4
 
Sensor holders GN 801. 3 and GN 801. 4 are designed as accessories for GN 810 and GN 820 series toggle clamps and enable contactless monitoring of the clamping positions using an inductive sensor.
 
When the clamping lever is in clamping position, the sensor electronics provide a high signal, e.g. to a machine control unit, and additionally indicate this switch status with an LED on the sensor.
 
 
Go to the Current Press Release!
GN 801.3ff
 
 
 
NEW  Rail Mounting Clamps GN 474.2
 
GN 474.2
Rail mounting clamps GN 474. 2 connect tubes and rods in parallel or at right angles. They are used for applications such as side guides, where the mounting clamps must not protrude to the side.
 
In addition, the split clamping point permits subsequent insertion of the mounting clamp into an existing structure and simplifies installation when axial insertion is not possible, such as due to curves.
 
More Information!
 
 
 
Upcoming Trade Shows
 
We look forward to seeing you at the following trade shows, where we can offer personalized advice and demonstrations of our products.
We will be exhibit at the following trade shows in February and March:
 
all about automation in Friedrichshafen
02/25/25 - 02/26/25
Booth B2-317
 
INTEC in Leipzig
03/11/25 - 03/14/25
Hall 2, Booth D07
 
Hannover Messe in Hanover
03/31/25 - 04/04/25
Hall 6, Booth E22
Tradeshows
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter