Newsletter
02/2020
 
 
Dear reader,
 
In today´s newsletter you will discover our new additions to the range of Stainless Steel-Indexing plungers. Corrosion resistant Stainless Steel is gaining in importance, which is why we offer different standard parts in Stainless Steel A4.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Stainless Steel-Indexing Plungers GN 818 in A4
 
GN 818 Stainless Steel-Indexing plungers can be used in particularly corrosive environments due to the materials used.
 
The indexing plungers are available with or without rest position.
The version with rest position is used for such applications where the plunger has to stay in its retracted position. In that case, the knob is retracted and afterwards turned by 90 degrees.
 
More information can be found here.
Stainless Steel-indexing plungers GN 818
 
 
 
Standard Parts in Corrosion Resistant Stainless Steel A4
 
Standard Parts in Corrosive Resistance Stainless Steel A4
 
Increased resistance in aggressive environments is becoming an increasingly important requirement in different industries. Therefore, corrosion resistant Stainless Steel A4 is gaining more and more meaning. The material represents a long service life with no maintenance and provides an added investment security.
 
Stainless Steel A4 is not only designed for use in corrosive atmospheres, but also for the food and medical industries.
 
See all Stainless Steel A4 products here. 
 
 
 
Upcoming Trade Shows
 
We look forward to seeing you at the following March trade fairs where we offer face to face advice and demonstrations of our products.
 
PACK EXPO East in Philadelphia, United States
represented by JW Winco
03/03/20 - 03/05/20
Booth 1217
 
Prolight + Sound in Frankfurt, Germany
03/31/20 - 04/03/20
Hall 12.0, Booth A63
 
analytica in Munich, Germany
03/31/20 - 04/03/20
Hall B2, Booth 328
Upcoming Trade Shows
 
 
 
Ganter services: 24h delivery
 
Fast and direct! Thanks to a streamlined logistics concept, Ganter is capable of delivering standard parts at extremely short notice – anywhere in the world.
 
learn more
 
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter