Newsletter
03/2021
 
 
Dear reader,
 
Indexing plungers secure various components quickly and reliably. For greater security against accidental release or manipulation, Ganter has developed the new lockable stainless steel indexing plungers GN 814.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Lockable Stainless Steel Indexing Plungers GN 814
 
Lockable stainless steel indexing plungers GN 814 are used for applications where unauthorized operation is to be prevented.
 
Depending on the type, the plunger pin is secured in the front or additionally in the rear position.
 
The supplied key can be removed in the end positions. This means that an accidental actuation of the indexing plunger is no longer possible after locking.
 
Learn more here.
Lockable Stainless Steel Indexing Plungers GN 814
 
 
 
Video  Clamping Levers with Eccentrical Cam GN 927
 
Clamping Levers with Eccentrical Cam
Clamping levers with eccentrical cam GN 927 are used for rapid clamping and releasing. In contrast to a clamping operation utilizing only threads, these levers permit a torque-free clamping.
 
The application video shows you how easily the clamping levers with eccentrical cam can be used.
 
You can find more clamping levers with eccentrical cam in different materials here.
 
 
 
Get started with Ganter for technical colleges and universities
 
The future of technology: To help ambitious technical projects become a reality, Ganter supports technical colleges and universities with standard parts and expertise.
 
learn more
 
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter