Newsletter
11/2022
 
 
Dear reader,
 
Ergonomic, highly functional and visually at its best. With the new stainless steel design series, Ganter sets the tone - and receives the German Design Award as well as the iF Design Award.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
Two Design Awards for Ganter 
 
Designawards
 
Design ensures a brand-appropriate product appearance, optimizes functionality and ergonomics, and even lowers the costs of production and operation.
 
Ganter proves just how positive an effective design can have with a new design series that the market leader from Furtwangen has developed together with the design agency Corpus-C. The series made of stainless steel AISI 316L consists of the GN 5063 T-handle, the GN 8340 wing nuts and the GN 8350 wing screws, the latter equipped with internal or external threads from M5 to M12.
 
The jury of the iF Design Award particularly emphasized the "outstanding ergonomic properties" as well as the "timeless" and "very high-quality" aesthetics.
 
More information can be found in the latest press release.
 
 
 
Follow us on LinkedIn 
 
On LinkedIn we regularly inform you about products and their application as well as helpful, technical information.
 
LinkedIn
 
 
 
Get started with Ganter for technical colleges and universities
 
The future of technology: To help ambitious technical projects become a reality, Ganter supports technical colleges and universities with standard parts and expertise.
 
learn more
 
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter