Newsletter
03/2025
 
 
Dear reader,
 
Spring brings a breath of fresh air to our product range:
Discover our high-quality snap latches, new locking pin extensions and versatile pneumatic clamps.
You'll find everything you need to know in this newsletter.
 
Have fun discovering!
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Snap Latches GN 449.5
 
Snap latches GN 449. 5 combine the function of a gripping tray with that of a snap latch to provide an easy way to keep doors, covers and hoods closed.
 
Once the mounting hole has been drilled, the housing is inserted into the hole in the door body when actuated and the mounting ring is pushed on from behind. The housing and mounting ring are connected with two supplied pan head screws.
 
More information
GN 449.5
 
 
 
NEW  Locking Pin with Axial Lock
 
GN 114
Ganter is expanding its range: in addition to the locking pins with axial lock and round knob, there are now also variants with L- or T-handles - both in steel and stainless steel.
 
Locking pins GN 114. 7 / GN 114. 8 / GN 114. 11 / GN 114. 12 with axial lock are used to quickly fix, connect and secure various components. Typically, they are used as bearing bolts that have to be frequently assembled and disassembled.
 
Find out more
 
 
 
Automation of the Clamping Action
 
Pneumaikspanner
 
Ganter offers a large selection of pneumatically operated clamps, power clamps and swing clamps. They differ primarily in terms of their clamping principle, size, ease of operation and holding force.
Pneumatically operated toggle clamps: These clamps are technically identical to manual toggle clamps, except that the clamping mechanism is actuated by a pneumatic cylinder.
Power clamps: These pneumatically operated clamps feature a high clamping force together with compact dimensions.
Swing clamps: These pneumatically operated clamps are used when the clamping point must be freely accessible for inserting and removing the workpiece. The clamping action is divided into a swinging movement of the clamping arm and a linear clamping motion.
 
To our Pneumatically operated clamps
 
 
 
Upcoming Trade Shows
 
We will also be happy to present our new products to you in person at our trade fair stand.
You can find us at the following trade fairs in March and April:
 
Hannover Messe
31.03.2025 to 04.04.2025
Hall 6, Booth E22
 
Bauma in Munich
07.04.2025 to 13.04.2025
Booth A6.409
 
Prolight + Sound in Frankfurt
08.04.2025 to 11.04.2025
Hall 12.0, Booth E90
Messekalender
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter