Newsletter
04/2021
 
Standard Parts. Ganter.
 
Dear reader,
 
Enlarging our range with additional new products creates further excitement on the standard parts market. Today, we give you an overview of just a few of our latest product developments.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Levelling Feet with Plastic Coated Base Plate
 
Levelling feet GN 30 and GN 32 can be used in a host of combinations of base plates and adjustable spindle versions.
 
The base plates of the steel levelling feet are now available with a black plastic coating (type A5).
 
The levelling feet GN 32 can be screwed to the mounting surface using the mounting flange, which prevents lateral shifting.
 
Levelling Feet with Plastic Coated Base Plate
 
 
 
NEW  Spirit Levels with Adjustment and Cross-Measurement
 
Spirit levels with adjustment and cross-measurement
In digital times, they seem like relics from the past, but spirit levels remain indispensable tools in everyday industrial operations.
 
Ganter has now expanded its existing selection of bull’s eye and screw-on spirit levels with two new models: Cross spirit levels GN 2276 and screw-on spirit levels GN 2283 – both as practical as ever.
 
Find more information in the current press release.
 
 
 
Nuevo Español | Nouveau Français | Uutuus Suomeksi 
 
We focus on internationality and have therefore expanded the language range on our website!
 
In addition to German and English, also Spanish, French and Finnish are now available to select.
Additional Website Languages
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter