Newsletter
06/2023
 
 
Dear reader,
 
Take a look at our June newsletter and discover some interesting news about our standard parts. Today we are introducing our new rod, disk and rectangular shaped retaining magnets.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Retaining Magnets of Special Quality
 
Retaining magnets GN 50. 8 are combined with the stainless steel housing into a system that shields and strengthens the magnet for optimal transmission of the magnetic flux onto the magnetic surface.
 
Because the stainless steel housing is tightly welded, the retaining magnets are suited for use in corrosive environments.
 
Thanks to the high temperature resistance up to 350 °C, the magnets can even be used on oven doors, for example.
 
Explore more
GN 50.8
 
 
 
NEW  Retaining Magnets with Gummed Magnetic Surface
 
GN 52.5 and GN 52.6 Combi
Retaining magnets GN 52. 5 and our new GN 52. 6 are combined with the stainless steel housing and the plastic ring into a system that shields and strengthens the magnet for optimal transmission of the magnetic flux onto the gummed magnetic surface.
 
The rubber protects sensitive surfaces from being damaged by the magnet and also delivers a high friction coefficient resulting in high lateral displacement forces.
 
Click to learn more
 
 
 
NEW  Retaining Magnets with Perfect Surface Protection
 
The retaining magnets GN 57. 3 with rubber jacket form a system together with the steel part that shields and strengthens the magnet, optimally concentrating the magnetic flux on the rubberized magnetic surface.
 
In addition to the retaining magnets with threaded stud, Ganter also offers a version with internal thread in the form of the retaining magnet GN 57. 1.
 
More Information
GN 57.1 and GN 57.3 Combi
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter