Newsletter
02/2022
 
Standard Parts. Ganter.
 
Dear reader,
 
Please see the enclosed February issue of the Ganter e-newsletter and discover interesting news about our standard parts.
We are pleased to present more EHEDG certified screws in today's newsletter.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
EHEDG Certification for Screws in Hygienic Design
 
In addition to the already certified stainless steel screws and nuts GN 1580, stainless steel screws GN 1581 with low-profile head as well as GN 1582 with recessed stud for loss protection are now also EHEDG certified.
 
The high-quality finish (Ra < 0.8 µm) as well as the large corner radii and closed surfaces prevent adherence of dirt and facilitate cleaning.
 
You can find more information about Hygienic Design here...
EHEDG Certification for Screws in Hygienic Design
 
 
 
NEW  Magnets GN 53.2 / GN 53.3 / GN 53.4
 
Magnets GN 53.2 / GN 53.3 / GN 53.4
These new magnets with neodymium magnets are used to hold documents, templates and drawings in the technical environment.
 
The magnet GN 53. 2 has a flat plastic housing in rectangular shape with two magnets.
 
The two round magnets GN 53. 3 and GN 53. 4 are equipped with an ergonomical handle made of plastic or steel.
 
All magnets in the Ganter portfolio can be found here...
 
 
 
Follow us on LinkedIn 
 
On LinkedIn we regularly inform you about products and their application as well as helpful, technical information.
Follow us on LinkedIn
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter