Newsletter
07/2022
 
Standard Parts. Ganter.
 
Dear reader,
 
In today's newsletter you will discover our range extensions in the field of stainless steel locking plungers. Corrosion resistant stainless steel is gaining more and more importance in various fields, which is why we offer the most diverse standard parts in stainless steel AISI 316.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Stainless Steel Locking Plungers GN 514 in AISI 316
 
Stainless steel locking plungers GN 514 can be used in particularly corrosive environments due to the materials used.
 
These locking plungers feature a functional mechanism based on the principle of a retractable pen. They offer very ergonomic operation that only requires pressing the knob once to put the plunger in the lock position and pressing the knob a second time to put the plunger in the unlock position.
 
More information can be found here.
Stainless Steel Locking Plungers GN 514
 
 
 
Standard Parts in Stainless Steel AISI 316
 
Standard Parts in Stainless Steel AISI 316
 
Increased resistance in aggressive environments is becoming an increasingly important requirement in different industries. Therefore, corrosion resistant stainless steel AISI 316 is gaining more and more understanding. The material represents a long service life with no maintenance and provides an added investment security.
 
Stainless steel AISI 316 is not only designed for use in corrosive environments but also for the food and medical industries.
 
See all stainless steel AISI 316 products here.
 
 
 
Our Ganter Catalogue
 
Ganter Catalogue 18.0
More than 60,000 standard parts can be found in the current catalogue 18.0, proven longsellers as well as brand new parts - including couplings, concealed multiple-joint hinges and standard parts in Hygienic Design.
We are sure that our catalogue will make your work easier and support you even better in selecting the right standard parts.
 
Request for free
 
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter