Newsletter
01/2025
 
 
Dear reader,
 
We hope you have had a good start to the new year! We wish you every success in 2025. To kick off the new year, we have some exciting new products for you! In our first newsletter, we present the new rail t-mounting clamps GN 476.2 and the extension of our sheet metal hinges GN 136.
Also find out which trade shows you can meet us in February.
 
We look forward to another year of successful cooperation. If you have any questions, please do not hesitate to contact us.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Rail T-Mounting Clamps GN 476.2
 
Rail T-mounting clamps GN 476. 2 connect tubes and rods in a T shape. They are used for applications such as side guides, where the mounting clamps must not protrude to the side.
 
In addition, the split clamping point permits subsequent insertion of the mounting clamp into an existing structure and simplifies installation when axial insertion is not possible, such as due to curves.
 
 
Learn More!
GN 476.2
 
 
 
Extension  Sheet Metal Hinges GN 136
 
GN 136
Sheet metal hinges GN 136 are available in many different versions and are suitable for light to medium-duty applications.
 
Ganter now also offers type B (with through-holes) in a new stainless steel version with a black powder coating (NISW). This variant is used when reflections and glare from the shiny surface are undesirable. The stainless steel hinges (NI) were used as the basis for the coated hinges so that corrosion protection is still guaranteed.
 
More Information!
 
 
 
Upcoming Trade Shows
 
We look forward to seeing you at the following trade shows, where we can offer personalized advice and demonstrations of our products.
We will be exhibit at the following trade shows in February:
 
all about automation in Friedrichshafen
02/25/25 - 02/26/25
Booth B2-317
 
WestPack in Anaheim, United States
represented by J.W. Winco, Inc.
02/05/25 - 02/06/25
Booth 5061
 
Expo Manufactura in Monterrey, Mexico
represented by JW Winco México, S.A.
02/11/25 - 02/13/25
Booth 2237
Trade Shows
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter