Newsletter
05/2024
 
 
Dear reader,
 
We are pleased to present practical innovations from Ganter in this newsletter. Our new indexing plungers with chamfered pin are finally here! We have also extended our range of lashing straps to include stainless steel versions.
 
We will be attending several trade shows in June and look forward to meeting you in person. Visit us and discover our latest innovations!
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Indexing Plungers with Chamfered Pin
 
Indexin Plungers
Indexing plungers GN 724. 4, GN 724. 5 and GN 724. 6 have a plunger pin with square cross-section, a latching surface on one side and a chamfer on the other. When the object to be secured moves towards the chamfer, the plunger pin is pushed back into the guide, allowing grooves and edges to pass over the pin. The plunger pin engages automatically in the direction of the latching surface.
 
 
More Information
 
 
 
NEW  Lashing Straps GN 1110 with Stainless Steel Buckle
 
Lashing straps GN 1110 are used in various applications to tightly fasten and secure material.
 
Due to the simple buckle, which can be released with the touch of one finger, the lashing strap is perfect for fixing cable bundles on machines or other components.
 
Ganter is now extending its range: the new high-quality stainless steel versions are now available in addition to the proven steel versions.
 
More Information!
GN 1110
 
 
 
Upcoming Trade Shows
 
We look forward to seeing you at the following trade show in June, where we offer face-to-face advice and demonstrations of our products:
 
ACHEMA in Frankfurt
06/10/24 - 06/14/24
Hall 11.0, Booth C 35
 
all about automation in Straubing
06/26/24 - 06/27/24
Booth J 217
Trade Shows
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter