Newsletter
06/2024
 
 
Dear reader,
 
In the June issue of the Ganter newsletter, we are delighted to present our latest product familiy within our extensive range of over 70,000 standard parts: Trapezoidal Lead Screws and Trapezoidal Lead Nuts
 
Discover our immediately available trapezoidal lead screws and the matching trapezoidal lead nuts
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Trapezoidal Lead Screws GN 103
 
In connection with trapezoidal lead nuts, trapezoidal lead screws GN 103 convert rotational movements into linear movements. They are used to move parts and transmit forces, such as in mechanical and plant engineering.
 
 
More Information!
GN 103
 
 
 
NEW  Trapezoidal Lead Nuts
 
GN 103x
Trapezoidal lead nuts GN 103. 1, GN 103. 2 and GN 103. 3 are used together with trapezoidal lead screws GN 103.
 
To minimize wear, the trapezoidal lead nuts should be lubricated. However, if lubrication is insufficient, the bronze alloy (gunmetal) generally has emergency running properties. Steel and stainless steel nuts are primarily used for sporadic adjustments.
 
Learn more!
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter