Newsletter
06/2020
 
 
Dear reader,
 
Innovations in the areas of adjusting screws and indexing plungers are constantly expanding our range to meet the growing needs of the standard parts market.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Stainless Steel-Adjusting Screws and Bearing Blocks
 
Stainless Steel-Adjusting screws GN 827 are used in combination with bearing blocks GN 828 for simple adjustment and positioning.
 
Simple adjustments can be made when using the adjusting screws in connection with the bearing blocks. They are ideally suited for various assemblies where devices have to be changed and positioned repeatedly.
 
More information can be found here.
GN 827 / GN 828
 
 
 
NEW  Indexing Plungers for welding and mounting
 
GN 722.4 / GN 722.5 / GN 722.6
With the new indexing plungers GN 722. 5 and GN 722. 6 with flange and GN 722. 4 for welding, the locking pin is actuated via the pull ring. This is done by hand, alternatively also by using an extended handle bar with hook.
 
The dimensional tolerances between the pin and the guide are designed so that it functions reliably even when contaminated.
 
The indexing plungers are available in Stainless Steel A4 and Steel.
 
 
 
NEW  Indexing Plungers GN 817.6 with Sensor
 
Indexing plungers very often fulfill safety functions – but this is not the only time when it is important to obtain feedback about their position. With the new series GN 817. 6, Ganter now also allows automated status checks.
 
The sensor electronics output a signal to a machine control and indicate the switch state with an LED on the sensor.
 
More information can be found in the current press release.
GN 817.6 Stainless Steel-Indexing plungers
 
 
 
Ganter services: 24h delivery
 
Fast and direct! Thanks to a streamlined logistics concept, Ganter is capable of delivering standard parts at extremely short notice – anywhere in the world.
 
learn more
 
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter