Newsletter
07/2023
 
 
Dear reader,
 
In this last newsletter before the summer break we present you two interesting new products. Hinges for Panels GN 938 and Snap Latches GN 449.4.
 
Greetings from the Black Forest!
Otto Ganter GmbH & Co. KG
 
 
 
NEW  Hinges for Panels GN 938
 
GN 938
Hinges GN 938 are used to fasten door panes, made of glass or plastic, so that they can rotate. They are designed to match the panel support clamp GN 939.
 
The panels (door panes) are clamped between the rubber inserts and additionally secured with spacer sleeves, forming a positive connection.
 
If the hinges are used with profile systems with 6, 8 or 10 mm slots, T-nuts GN 938. 1 are available as mounting accessories. These make it easy to align the hinges and protect them from twisting.
 
Get to know GN 938!
 
 
 
NEW  Snap Latches GN 449.4
 
Snap latches GN 449. 4 combine the function of a gripping tray with that of a snap latch to provide an easy way to keep doors and covers closed.
 
The mounting hole must be created according to the dimensions specified in the mounting information. For mounting, first insert the front body into the hole in the door, then push in the housing from the opposite side. Use the two supplied self-tapping screws to join the housing with the front body.
 
Learn More
GN 449.4
 
 
 
Follow us on LinkedIn 
 
On LinkedIn we regularly inform you about products and their application as well as helpful, technical information.
LinkedIn
 
 
Service
 
If you would like to unsubscribe from this newsletter, please click here.
 
 
 
Imprint
 
Otto Ganter GmbH & Co. KG
Triberger Straße 3, 78120 Furtwangen
Telefon +49 7723 6507-0, Telefax +49 7723 4659
www.ganternorm.com, info@ganternorm.com
 
Responsible for the contents is Axel Weber.
 
Otto Ganter GmbH & Co. KG
Headquarters: Furtwangen
Registered court: Freiburg, HRA
610300
UST.-IdNr.: DE 141912543
 
Personal liable partner:
Otto Ganter, Normteilefabrik Geschäftsführungs-GmbH
Headquarters: Furtwangen
Registered court: Freiburg, HRB 611562
Managing director: Stefan Ganter